You are here: Tools > AKD into KAS > Workbench Reference > AIN.ISCALE

AIN.ISCALE

General Information

Type

NV Parameter

Description

Sets the analog current scale factor.

Units

A/V

Range

0.001 to 22.4 A/V

Default Value

0.001 A/V

Data Type

Float

Start Version

M_01-01-01-000

Variants Supported

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5002h/0

M_01-01-01-000

Description

AIN.ISCALE sets the analog current scale factor that scales the analog input (AIN.VALUE) for DRV.OPMODE on pg. 1 = 1 (analog torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode).

The value entered is the motor current per 10 V of analog input. This value may be either higher or lower than 100%, but the actual analog input will be limited by the application current limit (IL.LIMITN on pg. 1 and IL.LIMITP on pg. 1).

Related Topics

Analog Input on pg. 1

Block Diagram for Position/Velocity Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™