You are here: Tools > AKD into KAS > Workbench Reference > IL.FOLDFTHRESHU

IL.FOLDFTHRESHU

General Information

Type

NV Parameter

Description

Sets the user value for the foldback fault level.

Units

Arms

Range

0 to 500 Arms

Default Value

DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK)

Data Type

Float

See Also

IL.FOLDFTHRESH on pg. 1, Foldback on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3421h/0

M_01-00-00-000

Description

IL.FOLDFTHRESHU is the fault level of the current foldback algorithm. The value of IL.FOLDFTHRESH is the minimum of DRV.IPEAK on pg. 1, MOTOR.IPEAK on pg. 1, and IL.FOLDFTHRESHU.

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™