You are here: Tools > AKD into KAS > Workbench Reference > PL.ERR

PL.ERR

General Information

Type

R/O Parameter

Description

Reads the position error present when the drive is controlling the position loop.

Units

counts, rad, deg, (custom units)

Range

N/A  

Default Value

N/A

Data Type

Float

See Also

PL.FB on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

35C5h/0

Profile specific SDOs/0

M_01-00-00-000

Description

PL.ERR reads the position error present when the drive is controlling the position loop. PL.ERR is the difference between the actual position of the motor shaft (PL.FB on pg. 1) and the commanded position of the drive (PL.CMD on pg. 1).  If the drive is not in the position operating mode (DRV.OPMODE on pg. 1 = 2), then the PL.ERR value is not generated by the drive and this parameter is read as 0.

Related Topics

PL.ERRFTHRESH on pg. 1 | PL.ERRMODE on pg. 1 | PL.ERRWTHRESH on pg. 1

Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™