You are here: Tools > AKD into KAS > Workbench User Guide > Position Loop

Position Loop

Overview

The position loop is active when the drive operates in position mode (DRV.OPMODE on pg. 1 = 2). The parameters that govern the position loop are shown in the Position Loop view. The various types of tuning inside AKD adjust these parameters, so you normally do not need to adjust the position loop parameters in the position loop screen.

Tabs in the Position Loop View

The position loop view includes an active block diagram. If you click on a block in the diagram, the appropriate tab opens below.

Position Loop Default Behavior and Changes

By default, only a proportional gain (PL.KP on pg. 1) is applied in the position loop.

 

Position Loop Changes Based on Slider Tuning

Slider Tuning (see Slider Tuning on pg. 1) adjusts the proportional gain of the position loop (along with velocity loop view parameters; see Velocity Loop on pg. 1). If you adjust the bandwidthIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz using the slider tuner, then when you return to the position loop screen, you will see a change to the proportional gain only. No adjustment is made to the integral gain or feedforward gain through the slider tuner. The integral saturation levels are not applicable when the integral gain is set to 0. In the Gains tab, the boxes for these values may be populated with default values whether or not the integral gain is set to 0.

Related Parameters

PL Parameters on pg. 1

DRV.OPMODE on pg. 1

VL.CMD on pg. 1

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™