You are here: Tools > AKD into KAS > Workbench Reference > VL.CMD

VL.CMD

General Information

Type

R/O Parameter

Description

Reads the actual velocity command; active in opmodes 1 (velocity) and 2 (position) only.

Units

Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1)

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

Range

N/A

Default Value

N/A

Data Type

Float

See Also

VL.FB on pg. 1, VL.CMDU on pg. 1, VL.LIMITP on pg. 1, VL.LIMITN on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

606Bh/0

M_01-00-00-000

Description

VL.CMD returns the actual velocity command as it is received in the velocity loop entry after all velocity limits (such as VL.LIMITN on pg. 1 and VL.LIMITP on pg. 1). See velocity loop design diagram for more details.

Related Topics

Velocity Loop

Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™