|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
Sets the user velocity command; active in opmodes 1 (velocity) and 2 (position) only. |
|
Units |
Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1) Rotary: rpm, rps, deg/s, custom units/s, rad/s Linear: counts/s, mm/s, µm/s, custom units/s |
|
Range |
Rotary -15,000.000 to 15,000.000 rpm -250.000 to 250.000 rps -90000.000 to 90000.000 deg/s -1250.000 to 1250.000 custom units/s -1570.796 to 1570.796 rad/s Linear -1,073,741,824,000.000 to 1,073,741,824,000.000 counts/s -8,000.000 to 8,000.000 mm/s -8,000,000.000 to 8,000,000.000 µm/s -1,250.000 to 1,250.000 custom units/s |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
VL.FB on pg. 1, VL.CMD on pg. 1, DRV.OPMODE on pg. 1, DRV.CMDSOURCE on pg. 1, VL.LIMITN on pg. 1, VL.LIMITP on pg. 1 |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
M_01-00-00-000 |
Description
VL.CMDU sets the user velocity command. When DRV.OPMODE on pg. 1 is set to 1 (velocity loop) and DRV.CMDSOURCE on pg. 1 is set to 0 (TCP/IP channel), then setting this value when the drive is enabled will cause the drive to rotate at the required velocity.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|