You are here: Tools > AKD into KAS > Workbench Reference > WS.IMAX

WS.IMAX

General Information

Type

R/W Parameter

Description

Sets maximum current used for wake and shake.

Units

Arms

Range

0 to (lower value of MOTOR.IPEAK and DRV.IPEAK) Arms

Default Value

(half of maximum) Arms

Data Type

U16

See Also

MOTOR.IPEAK on pg. 1, DRV.IPEAK on pg. 1

Start Version

M_01-01-00-101, M_01-02-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3494h on pg. 1/1

M_01-00-00-000

Description

This parameter defines the maximum current used for wake and shake. If the selected current is too low, the minimum required movement may not occur. If the selected current is too high, the movement may be too fast (overspeed) or too large (over maximum movement).

The maximum of this parameter is the lower value of MOTOR.IPEAK and DRV.IPEAK. The default value of this parameter is the half of its maximum. This value depends on the specific application.

Related Topics

Wake and Shake Overview on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™