You are here: Technical References > Programming Languages > PLC Standard Libraries > Basic Operations

Basic Operations

Below are the language features for basic data manipulation:

Below are the language features for controlling the execution of a program:

Below are the structured statements for controlling the execution of a program:

IF Conditional execution of statements.
WHILE Repeat statements while a condition is TRUE.
REPEAT Repeat statements until a condition is TRUE.
FOR Execute iterations of statements.
CASE Switch to one of various possible statements.
EXIT Exit from a loop instruction.
WAIT Delay program execution.
ON Conditional execution.

 

Assignment

Bit Access

Calling a Function

Calling a Function Block

Differences Between Functions and Function Blocks

Calling a Sub-program

CASE OF ELSE END_CASE

COUNTOF

DEC

EXIT

FOR TO BY END_FOR

IF THEN ELSE ELSIF END_IF

INC

Jumps JMP JMPC JMPNC JMPCN

Labels

MOVEBLOCK

Neg Integer Negation

ON

Parenthesis

REPEAT UNTIL END_REPEAT

RETURN RET RETC RETNC RETCN

WAIT / WAIT_TIME

WHILE DO END_WHILE


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™