You are here: Advanced Topics > Motion Bus and Fieldbuses > Fieldbus Editor > Profinet IO RT Controller Configuration

Profinet IO RT Controller Configuration

The KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger contains a fully integrated configurator for Profinet IO RT Controller.

The Profinet data size is limited to 500 bytes. To calculate the size, use the slot configuration view to count the number of bits per slot and convert to bytes. For example, 7 slots containing 16 outputs of 32 bits each, would be 7 * 16 * 32 = 3584 bits = 448 bytes.

 

Configuration

Data types

Additional features

How to resolve errors

Coding of PNIO status


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™