You are here: Technical References > Programming Languages > ST Language

Structured Text (ST)

ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal is a structured literal programming language. A ST program is a list of statements. Each statement describes an action and must end with a semi-colon (";").

The presentation of the text has no meaning for a ST program. You can insert blank characters and line breaks where you want in the program text.

Comments

Comment texts can be entered anywhere in a ST program. Comment texts have no meaning for the execution of the program. A comment text must begin with "(*" and end with "*)". Comments can be entered on several lines (i.e. a comment text can include line breaks). Comment texts cannot be nested.

You can also use // to add a comment on a single line as shown below:

//My main comment

(* My comment *)

a := d + e;

(* A comment can also

be on several lines *)

b := d * e;

 

c := d - e; (* My comment *)

 

Expressions

Each statement describes an action and can include evaluation of complex expressions. An expression is evaluated:

- from the left to the right
- according to the default priority order of operators
- the default priority can be changed using parentheses

Arguments of an expression can be:
- declared variables
- constant expressions
- function calls

Statements

Below are available basic statements that can be entered in a ST program:

- assignment
- function block calling

Below are the available conditional statements in ST language:

- IF / THEN / ELSE
   Simple binary switch.
   One or several ELSIF are allowed.

IF a = b THEN

   c := 0;

ELSIF a < b THEN

   c := 1;

ELSE

   c := -1;

END_IF;

 

- CASE
  Switch between enumerated statements according to an expression.
  The selector can be any integer or a STRING.

CASE iChoice OF

0:

MyString := 'Nothing';

1 .. 2,5:

MyString := 'First case';

3,4:

MyString := 'Second case';

ELSE

MyString := 'Other case';

END_CASE;

 

Below are the available statements for describing loops in ST language:

- WHILE
  Repeat a list of statements.
  Condition is evaluated on loop entry before the statements.

iCount := 0;

WHILE iCount < 100 DO

iCount := iCount +1;

MyVar := MyVar + 1;

END_WHILE;

 

- REPEAT
  Repeat a list of statements.
  Condition is evaluated on loop exit after the statements.

iCount := 0;

REPEAT

MyVar := MyVar + 1;

iCount := iCount + 1;

UNTIL iCount < 100 END_REPEAT;

 

- FOR
  Iteration of statement execution.
  The BY statement is optional (default value is 1)

FOR iCount := 0 TO 100 BY 2 DO

MyVar := MyVar + 1;

END_FOR;

 

Below are some other statements in ST language:

- WAIT / WAIT_TIME (suspend the execution)

- ON … DO (conditional execution of statements: provides a simpler syntax for checking the rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge of a Boolean condition)

 

Related Topics

Structured Text (ST) / Instruction List (IL) Editor

ST Editor Keyboard Shortcuts

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™