|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
NA |
|
Range |
4 to 19 |
|
Default Value |
19 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
Variants Supported
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5019h/0 |
M_01-00-00-000 |
Description
BODE.PRBDEPTH sets the length of the PRB signal before it repeats. This applies only when BODE.MODE = PRB. The PRB excitation will repeat after (2^BODE.PRBDEPTH) / BODE.EXCITEGAP drive samples.
Example
Set BODE.PRBDEPTH to 19:
-->BODE.PRBDEPTH 19
Get BODE.PRBDEPTH (already set to 19):
-->BODE.PRBDEPTH 19
Related Topics
Using the Performance Servo Tuner
Using the Performance Servo Tuner: Advanced
Error: Invalid Bode plot mode for this function.
BODE.MODE, BODE.INJECTPOINT, BODE.IAMP, BODE.VAMP
|
Copyright © 2015 Kollmorgen™ |
|