|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3451h/0 |
M_01-00-00-000 |
Description
This parameter determines whether or not certain drive parameters (see lists below) are calculated automatically. When MOTOR.AUTOSET = 1 these parameters are automatically calculated from the motor ID data (read from memory-supporting feedback devices). Parameters loaded from motor memory are then read-only and cannot be modified as long as MOTOR.AUTOSET = 1. If MOTOR.AUTOSET = 0, parameters are not loaded from motor memory and must be configured by the user. Parameters which are not loaded from motor memory are always read-write.
Three conditions determine which parameters are calculated automatically by MOTOR.AUTOSET = 1. See the lists below to determine which parameters will automatically be configured from the motor ID data.
The following parameters may be configured automatically when MOTOR.AUTOSET = 1:
If the motor's FB1.MEMVER > 0.01, AKD will also configure:
For firmware versions 01-09-00-000 and later, AKD will also configure:
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|