BODE.MODE

General Information

Type

R/W Parameter

Description

Sets the mode of the excitation.

Units

N/A

Range

0 to 4

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Description

BODE.MODE sets the mode of the excitation. The excitation can be set to the modes shown in the table below. BODE.MODE is always set to None when EthernetEthernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) communication is disconnected. The peak amplitude of the excitation is set by either BODE.IAMP or BODE.VAMP (depending on BODE.INJECTPOINT).

BODE.MODE is subject to a watchdog timer (BODE.MODETIMER) as follows:

BODE.MODE

Description

Comments

0

None

Turns all excitation off

1

PRB

Uses Pseudo Random Binary (PRB) excitation. PRB is a signal that is always +/- peak amplitude, varying only in phase.

PRB excitation results in a flat excitation frequency spectrum. PRB results in a high peak excitation amplitude, which can help minimize friction in a frequency response test.

PRB excitation repeats every (2^BODE.PRBDEPTH) / BODE.EXCITEGAP drive samples. This repetition can be used to reveal the effects of friction.

2

Sine

Uses Sine excitation

3

Noise

Uses random noise excitation. Noise is a random number generator that varies between +/- peak amplitude.

4 Offset

Sets a torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist offset equal to BODE.IAMP

Example

Set BODE.MODE to PRB:

-->BODE.MODE 1

Get BODE.MODE (already set to PRB):

-->BODE.MODE 1

PRB excitation:

Sine excitation:

 

Noise excitation:

Related Topics

Using the Performance Servo Tuner

Using the Performance Servo Tuner: Advanced

Scope

Settings

F126 n126

Error: Invalid Bode plot mode for this function.

BODE.INJECTPOINTBODE.VAMP

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™