MLAxisPipePos
Description
Returns the pipe position of the axis.
-
- This function or function block returns cached data. See Programming a Dual Core Controller for more information.
Arguments
Input
|
ID |
Description |
ID Name of the Axis block |
|
Data type |
DINT |
|
|
Range |
[-2147483648, 2147483648] |
|
|
Unit |
n/a |
|
|
Default |
— |
Output
|
OK |
Description |
Returns true when function successfully executes See more details here |
|
Data type |
BOOL |
|
|
Unit |
n/a |
|
|
Position |
Description |
|
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
Related Functions
Example
Structured Text
|
Axis1_Pipe_Position := MLAxisPipePos (PipeNetwork.Axis1 ) ;
|
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|