MLAxisWritePipPos
Description
Force the pipe position internal value. This function is working only when no pipe is connected.
Arguments
Input
|
AxisID |
Description |
ID Name of the Axis block |
|
Data type |
DINT |
|
|
Range |
— |
|
|
Unit |
n/a |
|
|
Default |
— |
|
PipePosition |
Description |
Sets the Axis Pipe Position |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
||
|
Default |
— |
Output
|
Default (.Q) |
Description |
Returns true when function successfully executes See more details here |
|
Data type |
BOOL |
|
|
Unit |
n/a |
Related Functions
Example
Structured Text
|
MLAxisWritePipPos(PipeNetwork.Axis1, 3000 ) ;
|
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|