MLPrfWriteOOffset
Description
Changes the Output Offset value of a selected CAM Profile. Offsets are changed on the fly to modify the CAM Profile while maintaining its shape. A change in output offset is equivalent to shifting the CAM Profile on the Y (or Output) Axis.
Figure 10-84: MLPrfWriteOOffset
Arguments
Input
|
ProfileID |
Description |
ID number of an initialized CAM Profile |
|
Data type |
DINT |
|
|
Range |
[-2147483648, 2147483648] |
|
|
Unit |
n/a |
|
|
Default |
— |
|
|
Offset |
Description |
Desired new value of Output Offset |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
n/a |
|
|
Default |
— |
Output
|
Default (.Q) |
Description |
Returns TRUE if the Output Offset value is changed See more details here |
|
Data type |
BOOL |
|
|
Unit |
n/a |
Return Type
BOOL
Related Functions
Example
Structured Text
|
//Change value of output offset MLPrfWriteOOffset( Profiles.Profile_A , 45 );
|
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|