AXIS#.MOTOR.VMAX
Description
This parameter is the maximum motor mechanical speed. The value 1.2 x AXIS#.MOTOR.VMAX becomes the overall overspeed fault threshold (AXIS#.VL.VFTHRESH) if it is less than the user overspeed fault threshold (AXIS#.VL.THRESH ), and for AXIS#.MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).
-
-
This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
rpm |
|
Range |
100 to 40,000 rpm |
|
Default Value |
3,000 rpm |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.MOTOR.VMAX | 0x500B | 0x1F | UINT | - | - | RW | False |
| AXIS2.MOTOR.VMAX | 0x510B | 0x1F | UINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|