AXIS#.PL.ERRFTHRESH

Description

This parameter sets the maximum position error. If the position error AXIS#.PL.ERR is larger than AXIS#.PL.ERRFTHRESH the drive generates a fault. If AXIS#.PL.ERRFTHRESH is set to 0, the maximum position error is ignored.

Example

Set position rotary units to 2 (degrees). Setting AXIS#.PL.ERRFTHRESH to 1000 states that is the position error is larger than 1000 degrees, the drive will generate a fault.

AXIS#.UNIT.PROTARY 2

AXIS#.PL.ERRFTHRESH 1000

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

42949672960 counts

Note: Default is adjusted to account for the units selected by the user

Data Type

Float

See Also

AXIS#.PL.ERR

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.PL.ERRFTHRESH 0x500C 0x3 DINT - Position RW False
AXIS2.PL.ERRFTHRESH 0x510C 0x3 DINT - Position RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen