AXIS#.PL.ERR

Description

AXIS#.PL.ERR reads the position error present when the drive is controlling the position loop. AXIS#.PL.ERR is the difference between the actual position of the motor shaft (AXIS#.PL.FB ) and the commanded position of the drive (AXIS#.PL.CMD ).  If the drive is not in the position operating mode (AXIS#.OPMODE = 2), then the AXIS#.PL.ERR value is not generated by the drive and this parameter is read as 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

AXIS#.PL.FB

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

AXIS#.PL.ERRFTHRESH | | AXIS#.PL.ERRWTHRESH

Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen