FB#.IDENTIFIED
Description
This parameter is set according to FB#.SELECT on drive power up if FB#.SELECT is not –1; otherwise the parameter value is read from the drive memory.
|
Type |
Description |
|---|---|
|
0 |
Unknown |
| 1 | No encoder |
|
10 |
Incremental encoder with A/B Quad, marker pulse and Hall |
|
11 |
Incremental encoder with A/B Quad, marker pulse and no Hall |
| 13 | Step/Direction |
| 14 | Clockwise/Counter-clockwise |
|
20 |
Sine Encoder , with marker pulse and Hall |
|
21 |
Sine encoder , with marker pulse & No Halls |
|
30 |
EnDat 2.1 with Sine Cosine |
|
31 |
EnDat 2.2 |
|
34 |
|
|
40 |
Resolver |
|
41 |
|
| 45 | SFD3 |
| 46 | Hiperface DSL |
| 63 | Simulated Motor |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|