FB#.SELECT

Description

FB#.SELECT sets the feedback type manually (see FB#.IDENTIFIED ) or allows the drive to automatically identify the feedback type on power up.

Power Supply Notes:

If FB#.SELECT = -1, the power supply will only turn on during the initialization phase. If the feedback type cannot be automatically detected, the power supply will be turned off, and remain off until a AXIS#.CLRFAULTS is issued (which will re-start the FB initialization), or FB#.SELECT is manually set to a specific feedback type.

When FB#.SELECT is manually set to a specific feedback type, the FB power supply will remain on, unless a short is detected. This is useful for encoder types that may require calibration.

FB#.SELECT Input Values

Changing these input values will manually set the value of FB#.IDENTIFIED .


  • If the feedback setting fails, FB#.IDENTIFIED is automatically set to 0 (no feedback identified).

Input Value

Type

Notes

–1

Auto-identify The drive automatically identifies the type of feedback as part of the power up process. Note some feedback types cannot be automatically identified so the exact feedback needs to be selected. If auto identify is selected FB#.IDENTIFIED will be updated with the type of feedback found or 0 if no feedback can be found.
1 No Encoder Use this if no feedback deviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position is connected to the associated connector.

10

Incremental Encoder with Halls A/B Quadrature. Depending on the connector used the index pulse may not be supported.
11 Incremental Encoder without Halls A/B Quadrature. Depending on the connector used the index pulse may not be supported.
13 Step / Direction

-

14 CW / CCW Clockwise/Counter-Clockwise

20

Sine Encoder with Halls Depending on the connector used the index pulse may not be supported.
21 Sine Encoder without Halls Depending on the connector used the index pulse may not be supported.

30

EnDat 2.1 - Analog Uses the analog channels to track position. Can be used with any EnDat device that supports analog channels.

31

EnDat 2.2 - Digital Only uses serial communications to track position. Can be used with any EnDat device that support the 2.2 protocol.
34 BiSS"Bi-directional Serial Synchronous interface" An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder Mode C - Digital

The supported BiSS-C encoders are listed here:

https://www.kollmorgen.com/en-us/developer-network/what-types-biss-c-encoders-are-supported-akd-0/

40

Resolver -

41

SFD Smart Feedback DeviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position
45 SFD3

-

46 Hiperface DSL

-

Context

See Feedback.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

FB1 & FB2: -1, 1, 45, 46

FB3: -1, 1, 10, 11, 13, 14, 20, 21, 30, 31, 34, 40, 41

FB4 & FB5: 1, 11, 13, 14

Default Value

FB1 & FB2: -1

FB3, FB4, & FB5: 1

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen FB1.SELECT 0x3500 0x1 SINT - - RW False
FB2.SELECT 0x3501 0x1 SINT - - RW False
FB3.SELECT 0x3502 0x1 SINT - - RW False
FB4.SELECT 0x3503 0x1 SINT - - RW False
FB5.SELECT 0x3504 0x1 SINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen