FB#.LINEPITCH

Description

This parameter defines the line pitch for linear encoders in nm per line. Only used when using linear motor types.

Examples

Context

See Feedback and FB#.MECHTYPE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

nm/line

Range

1 to 4,294,967,295

Default Value

50

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen