FB#.MECHTYPE

Description

Sets whether the feedback is a rotary (0) or linear (1) encoder. If rotary, FB#.ENCLINES is the encoder resolution, and if linear, FB#.LINEPITCH is.

Depending on the configuration and feedback type, this parameter will be read only or read write. If used as a commutation feedback source for an axis (AXIS#.IL.FBSOURCE) this value will match AXIS#.MOTOR.TYPE for the corresponding axis. Otherwise, the value will match the feedback memory setting if available. Only if not assigned as an axis commutation source or unavailable through feedback memory will this value be settable by the user.

Context

See Feedback.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write or Read Only depending on configuration and feedback type

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen