IL.CMDACC
Description
Use IL"Instruction list" This is a low-level language and resembles assembly.CMDACC to monitor the commanded acceleration for a given motion. This keyword is useful for tuning acceleration feedforward (IL.KACCFF).
General Information
|
Type |
R/O Parameter |
|
Units |
Depends on UNIT.ACCLINEAR or UNIT.ACCROTARY. |
|
Range |
+/- 64bit |
|
Default Value |
0 |
|
Data Type |
Float |
|
Start Version |
M_01-08-03-000 |
|
Index/Subindex |
Is 64 bit? | Attributes | Signed? | |
|---|---|---|---|---|
|
1760 |
Yes | 64-bit | Yes |
Related Topics
|
Copyright © 2018 Kollmorgen |
|