MOTOR.TEMPC

Description

When the motor has a thermistor with linear characteristics (MOTOR.RTYPE = 2, 3 or 4), MOTOR.TEMPC returns the motor temperature in degrees Celsius, which is calculated from the resistance of the motor thermistor.

There is no algorithm to convert from resistance to degrees Celsius for non-linear thermistors. In this case, MOTOR.TEMPC returns -32,768 which is an invalid temperature.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-215 to 215

Default Value

N/A

Data Type

Integer

Start Version

M_01-10-04-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3458h/0

M_01-10-04-000

Related Topics

Motor | MOTOR.TEMP | MOTOR.RTYPE

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen