TEMP.POWER1 to TEMP.POWER3
Description
Reads the temperature of the power board(s) temperature sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer(s). Most AKDs have only one power board sensor which is read by TEMP.POWER1.
General Information
|
Type |
R/O Parameter |
|
Units |
Degrees Celsius |
|
Range |
-127 to 128 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-09-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|