Programming Languages - Overview
Below are the available programming languages of the IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 standard:
SFC: Sequential Function Chart
FBD: Function Block Diagram
FFLD: Free Form Ladder Diagram
ST: Structured Text
IL: Instruction List
Use of ST instructions in graphic languages
You have to select a language for each program or User-Defined Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. of the application.
Refer also to the following pages about the IEC 61131-3 programming languages:
Program organization units
Data types
Structures
Variables
Arrays
Constant expressions
Conditional compiling
Handling exceptions
|
Copyright © 2018 Kollmorgen |
|