FunctionMLAxisReadFBUnitPipe Network motion icon

Description

Get the feedback units per revolution value of the axis

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Output

OK

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

FBUnitsPerRev

Description

Returns the Axis Feedback Units per revolution

 

Data type

LREAL

 

Unit

n/a

Example

Structured Text

 

Axis1_Feedback_Units := MLAxisReadFBUnit(PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisReadFBUnit: LD example

Function Block Diagram

MLAxisReadFBUnit: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen