FunctionMLAxisWritePipPosPipe Network motion icon

Description

Force the pipe position internal value. This function is working only when no pipe is connected.

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

PipePosition

Description

Sets the Axis Pipe Position

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLAxisReadActPos

MLAxisFBackPos

MLAxisGenPos

MLAxisPipePos

MLAxisCmdPos

Example

Structured Text

 

MLAxisWritePipPos(PipeNetwork.Axis1, 3000 ) ;

 

Ladder Diagram

MLAxisWritePipPos: LD example

 

Function Block Diagram

MLAxisWritePipPos: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen