Skip To Main Content
  • placeholder
Filter:
Submit Search

FunctionECATGetObjVal


  • This function is deprecated as of KAS v2.7. The recommended best practice is to map a PLCClosed"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variable to a PDO object.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen