FunctionMLMotionCycleTimePLCopen motion iconPipe Network motion icon

Returns the Motion Base Cycle time in seconds.

Arguments

Input

Enable Description  
Data type  
Range  
Unit  
Default  

Output

OK Description  
Data type  
CycleTime Description Cycle time in seconds
Data type  
Unit  

Example

Structured Text

//Read EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs cycle rate in ms
lrCycleTime:= MLMotionCycleTime();

Ladder Diagram

Function Block Diagram

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen