FunctionMLPmpRelPipe Network motion icon

Description

This function is used to perform two subsequent relative moves. Using the MLPmpRel function block, the PMP Generator is capable of producing forward-backward motions with a non-stop, jerkClosedIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time-free transition through zero speed (see Figure below). This feature is frequently useful for linear axes which must move back and forward without any pause at one end.

This function can also be used to do a single relative move, ending in zero speed, by setting the DeltaSecond argument to zero (0.0). If it is done, for the controlling speed to be the first move, the “Last_Travel_Speed” parameter has to be set equal to or greater than the “First_Travel_Speed” parameter.

In general, the slower of the two “Speeds” is utilized to optimize the S-curve behavior for the move whether it is a 2 or 1 delta move.

If the DeltaSecond argument is non-zero, it must have the opposite sign than the sign of the DeltaFirst argument.

PMP Generator Forward & Backward Motion Profile

Figure 8-105: PMP Generator Forward & Backward Motion Profile

Arguments

Input

BlockID Description ID Name of the PMP function block in the Pipe Network
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit n/a
  Default —
DeltaFirst Description Length of first Move
  Data type LREAL
  Range —
  Unit User unit
  Default Value defined in the setup of a PMP Block within a Pipe Network. It is the “FIRST_TRAVEL_SPEED” field in the parameter tab.
DeltaSecond Description Length of second (return) Move
  Data type LREAL
  Range —
  Unit User unit
  Default Value defined in the setup of a PMP Block within a Pipe Network. It is the “LAST_TRAVEL_SPEED” field in the parameter tab.

Output

Default (.Q)

Description Returns True if the MLPmlRel successfully completed

See more details here

  Data type BOOL
  Unit n/a

Related Functions

MLPmpWriteAccel

MLPmpWriteFstSpd

MLPmpWriteJerk

MLPmpWriteLstSpd

Example

Structured Text

//Execute a Relative move on a PMP Block name “PmpMaster” with a First Travel Speed of 750.0, Second Travel Speed of -500,
MLPmpRel( PipeNetwork.PmpMaster, 750 , -500);

Ladder Diagram

MLPmpRel: LD example

Function Block Diagram

MLPmpRel: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen