FunctionMLMstAddPipe Network motion icon

Description

Performs a move for a specified distance relative to the endpoint of the previous move. Returns TRUE if the function succeeded.

Arguments

Input

EN

Description

Enables FB to be executed

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

—

Block ID

Description

ID name of the Master Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

DeltaPos

Description

Relative distance to move

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLMstWriteSpeed

MLMstWriteDecel

Example

Structured Text

//At the endpoint of the previous move, with the Master  pipe block named “MASTER”, make a move of 750.0
MLMstAdd( PipeNetwork.MASTER, 750.0 );

Ladder Diagram

MLMstAdd: LD example

Function Block Diagram

MLMstAdd: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen