udpRcvFromPLCopen motion icon

Description

This function receives a UDP telegram. If the characters are received, the function fills the ADD argument with the internal “UDP” of the sender. This buffer can then be passed to the udpSendTo function to send the answer.

Arguments

Input

En Description Execute the function
  Data type BOOL
  Range [0,1]
  Unit n/a
  Default —
sock Description ID of the socket
  Data type DINT
  Range [0,+65535]
  Unit n/a
  Default —
nb Description Maximum number of characters received
  Data type DINT
  Range [0,+65535]
  Unit n/a
  Default —
add[] Description Buffer containing the UDP address of the transmitter (filled on output)
  Data type USINT
  Range [0,32]
  Unit n/a
  Default —
data Description Buffer where to store received characters
  Data type STRING
  Range [0,255]
  Unit n/a
  Default —

Output

OK Description Returns true when the function successfully executes. See Function - General rules.
  Data type BOOL
  Unit n/a
Q Description Actual number of received characters
  Data type DINT
  Unit n/a

Examples

Structured Text

ReceivedBytes := udpRcvFrom(Socket_Number,5,add,data); //Read the position

Ladder Diagram

Function Block Diagram

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen