List of KAS Manuals

Find below the available literature for the following components:

KAS

KAS Title PDF Description
Release Notes The KAS version 3.02 Release Notes contain fixed limitations, known limitations, workarounds, and information on all hardware and software components that have been updated, changed or added in this release.
Getting Started

Covers the main steps to get your KAS system up and running

30 Minutes to Motion

Covers the main topics to help you start quickly with KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger. The objective is to familiarize you with the basic principles and the way the program works by creating a simple motion application project.

IDE User Manual Contains the content to help you with KAS IDE, except the topics included in the Reference Manuals
Reference Manual - PLCClosed"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Library Contains Technical References on PLC Programming Languages and Library
Reference Manual - Motion Library Contains Technical References on Motion Library for Pipe Network and PLCopenClosedA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML

Go back to the top of the page [Top]

KVB

KVB Guide   Description
Kollmorgen Visualization Builder™ Quick Start Guide Quick Start that covers the most important points to install and use Kollmorgen Visualization Builder, in order to configure HMI Panels and PC operated control applications
Kollmorgen Visualization Builder™ User Manual Contains all the content to help you with Kollmorgen Visualization Builder

Go back to the top of the page [Top]

HMI

HMI part number Description KVB Tech. Manual
AKI2G-CDA-MOD-05T-000, 5" LCD Display Graphical Display 7" TFT LCD, Touchscreen v2.20
AKI2G-CDA-MOD-07T-000, 7" LCD Display Graphical Display 5" TFT LCD, Touchscreen v2.20
AKI2G-CDB-MOD-07T-000, 7" LCD Display Graphical Display 7" TFT LCD, Touchscreen v2.20
AKI2G-CDB-MOD-12T-000, 12" LCD Display Graphical Display 12" TFT LCD, Touchscreen v2.20
AKI-CDC-MOD-12T-000 Graphical Display 12.1" TFT LCD, Touchscreen v2.0
AKI-CDC-MOD-15T-000 Graphical Display 15.4" TFT LCD, Touchscreen v2.0
AKI-CDC-MOD-21T-000 Graphical Display 21.5" TFT LCD, Touchscreen v2.0

Go back to the top of the page [Top]

I/O

I/O terminal part number Description Tech. Manual
AKT-AN-200-000 2 Channel Thermocouple Input Module
AKT-AN-400-000 4 Channel Thermocouple Input Module
AKT-AN-410-000 4 Channel Analog Input Module, 0-10 VDC
AKT-AN-420-000 4 Channel Analog Input Module, 0-20 mA
AKT-AN-810-000 8 Channel Analog Input Module, 0-10 VDC
AKT-AN-820-000 8 Channel Analog Input Module, 0-20 mA
ACCT-AT-220-000 2 Channel Analog Output Module, 0-20 mA
AKT-AT-410-000 4 Channel Analog Output Module, 0-10 VDC
AKT-AT-420-000 4 Channel Analog Output Module, 0-20 mA
AKT-AT-810-000 8 Channel Analog Output Module, 0-10 VDC
AKT-AT-820-000 8 Channel Analog Output Module, 0-20 mA
AKT-DN-004-000 4 Channel Digital Input Module, 24 VDC 3ms
AKT-DN-008-000 8 Channel Digital Input Module, 24 VDC 3ms
AKT-DNH-004-000 4 Channel Digital Input Module, 24 VDC 0.2ms
AKT-DNH-008-000 8 Channel Digital Input Module, 24 VDC 0.2ms
AKT-DT-004-000 4 Channel Digital Output Module, 24 VDC 0.5A
AKT-DT-008-000 8 Channel Digital Output Module, 24 VDC 0.5A
AKT-DT-2RT-000 2 Channel Relay Output Module, 230 V AC 2.0A Rel.2NO Pot.-Free
AKT-ECT-000-000 EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Bus Coupler
AKT-EM-000-000 Standard-Bus End Terminal
AKT-IM-000-000 Isolation / Separation Terminal
AKT-PS-024-000 Power Supply, 24 VDC
AKT-PSF-024-000 Fused Power Supply with diagnostics, 24 VDC
AKT-SM-L15-000 Stepper Motor Terminal, 24 VDC, 1.5 A
AKT-SM-L50-000 Stepper Motor Terminal, 50 VDC, 5 A

  • 24-volt power is not passed through AKT-AN-200-000 and AKT-AN-400-000 thermocouple modules. To get 24VDC power to devices that need it (such as an AKT_AT-410-000 Output module) there are two possible solutions. :

    • Place the module requiring 24VDC before the thermocouple module.
    • Add a power feed module (AKT-PS-024-000 or AKT-PSF-024-000) after the thermocouple module.

Go back to the top of the page [Top]

AKD

Drives Guide   Description
AKD Quick Start Contains all information needed to safely install and setup an AKD drive
AKD PDMM Installation Manual Covers the most important points to install the drive hardware and software
Provides instructions for basic drive setup and connection to a network
AKD User Manual Describes how to use your drive in common applications. It also provides tips for maximizing your system performance with the AKD
AKD2G Installation Manual  
AKD Accessories Manual Includes technical data and dimensional drawings of accessories such as cables, brake resistors, and mains supplies
AKD EtherCAT Manual Describes the installation, setup, range of functions, and software protocol for the EtherCAT AKD product series
AKD2G EtherCAT Manual  
S300 Reference Documentation Kollmorgen website that gives access to all S300Closed"Servostar 300 drive" See Servo Drive in Glossary manuals
S700 Reference Documentation Kollmorgen website that gives access to all S700Closed"Servostar 700 drive" See Servo Drive in Glossary manuals

Go back to the top of the page [Top]

PDMM / PCMM

Product Guide   Description
AKD PDMM Quick Start Contains all information needed to safely install and setup an AKD drive
AKD and AKD PDMM Installation Manual Covers the most important points to install the drive hardware and software
Provides instructions for basic drive setup and connection to a network
PCMM Installation Guide Covers the most installation and setup of the controller.
AKD PDMM User Guide Contains information on AKD drive parameters, EWV (Embedded Workbench Views), and using the AKD PDMM in the KAS IDE.
AKD PDMM Fault Card Includes technical data and dimensional drawings of accessories such as cables, brake resistors, and mains supplies

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen