Working with the Hardware
In some cases, using the buttons on the controller may be preferable to using the web server. On the front of the controller there are two buttons, B2 and B3. B2 is above B3. These buttons may be used to enter Recovery Mode (see "Booting from the Recovery Image"), Display the IP Address of a PDMM or PCMM, stop and start the application, reset the control to factory settings (see "Reset the Controller to Factory Settings"), and backup/restore the firmware.
| Result | Press and hold |
|---|---|
| B2 | Recovery Mode |
| B3 | Menu access |
Table 7-1: B2/B3 button functionality at start-up
| Press | Result |
|---|---|
| B2 | Menu option selector |
| B3 | Menu access |
|
Copyright © 2018 Kollmorgen |
|