Soft Oscilloscope

The soft oscilloscope (commonly known as "softscope" or "scope") is a tool which allows you to view, in a two-dimensional graph, one or more variables' evolution (vertical axis) across the time (horizontal axis).

The scope (as seen in Figure 7-22: Example of using the Oscilloscope) has a set of channels where each can acquire the evolution of a value. A value may be the feedback position of an axis, the speed of a machine, or anything else that can be measured with the oscilloscope probes. For details on how to assign a variable to a channel, see "Plugging Probes, Mapping Variables".

Scope View

Figure 7-22: Example of using the Oscilloscope

The soft oscilloscope is a child window in the workspace which has two visually distinct parts:

  • The Control Panel enables you to assign variables to a channel and to change the settings of the soft oscilloscope (including those of the channels)
  • The Graphical Area shows the traces (or variable values) acquired by the channels
  • The control panel and the graph are separated by a splitter which allows you to change the size of the two panes.

    • You can hide the control panel by dragging the splitter all the way to the left. To show the control panel again, click and drag the splitter to the right.

Access the Soft Oscilloscope

In order to access the softscope, select the Oscilloscope command from the Tools menu.

Accessing the Scope

Figure 7-23: Accessing the Scope

About OpenGL

For the Graphical Area, the scope uses OpenGLClosedOpenGL (Open Graphics Library) is a standard specification defining a cross-language, cross-platform API for writing applications that produce 2D and 3D computer graphics. The Softscope uses this API to implement graphical manipulations for performance reasons. If you encounter problems in the quality of drawings, we suggest that you consider the following points before contacting our support desk:


  • Disabling most or all OpenGL accelerations is compensated by an increase in CPU consumption. It can lead to a point where the soft oscilloscope is not very usable when limited hardware is trying to display loads of samples.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen