How Do I Export the Oscilloscope Data?

To copy the trace data into a CSV file:

  1. Display the softscope
  2. Ensure the channels you want to export are Enabled and Visible
  3. Start the data collection
  4. Wait for the probe data you want to save to be collected
  5. Stop the data collection
  6. Click the Export... button
  7. Select where you want to save the CSV file
  8. Click the Save button

You can now import the data into Microsoft Excel.


  • The Export operation is possible even when acquisition of samples is in progress. But in that case, the latest exported data are the data collected when you have defined the CSV file.


  • The acquisition of samples is limited to 100 s when the cycle time is set to 1000 µs (respectively 50 s with 500 µs, and 25 s with 250 µs)

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen