Cam Profile Switching
At pipe network start-up or when using the MLCamSwitch function block, a Cam block's output position is set to the output position of the initialized profile.
For example if the following profile is switched in and the present pipe network position at the input of the cam block is 150 the position at the output of the cam block will be 50. Then as the input to the Cam block increases or decreases the Cam output value wiill increase or decrease respectively. And it will go through the modulo without a postion jump.
|
Copyright © 2018 Kollmorgen |
|