FunctionMLCamSwitchPipe Network motion icon

Description

Switches the CAM Profile in a selected CAM object. Can be used in combination with a comparator to check that profiles are switched at a time where the input and output values of both the old and new profiles are equal, so an Axis receives continuous position values and does not jump.

These profiles are created and initiated separately and the shape is created with the CAM Editor. With the Editor profiles can be changed graphically or by manually changing values in a numeric table relating input and output values with specific slopes. The Cam Editor software tool provides the capability to visualize, analyze, edit, and smooth profiles.

See Cam Profile Switching for more information.

Arguments

Input

BlockID

Description

ID number of an initialized CAM Pipe Block

Data type

DINT

Range

[-2147483648, 2147483648]

Unit

n/a

Default

—

ProfileID

Description

Name of the new CAM profile which is assigned to the CAM Pipe Block. It must be a declared profile object.

Data type

DINT

Range

[-2147483648, 2147483648]

Unit

n/a

Default

—

Output

Default (.Q)

Description

Returns TRUE if the CAM Profile is changed

See more details here

Data type

BOOL

Unit

n/a

Return Type

BOOL

Related Functions

MLProfileCreate

MLProfileInit

MLPrfWriteIOffset

MLPrfWriteOScale

Example

Structured Text

 

//Switch CAM Profile

MLCamSwitch(PipeNetwork.CAM, Profiles.Profile_B);

 

Ladder Diagram

MLCamSwitch: LD example

Function Block Diagram

MLCamSwitch: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen