AXIS#.HOME.CREEPFACTOR
Description
AXIS#.HOME.CREEPFACTOR is the percentage of the homing speed (AXIS#.HOME.V) used when searching for the feedback’s index. AXIS#.HOME.CREEPFACTOR is only used in home modes 3, 6 and 10.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS, using either a PAC
"Programmable Automation Controller"
PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
|
Type |
Read/Write |
|
Units |
% |
|
Range |
1 to 100 |
|
Default Value |
50 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Related Topics
Homing
|
Copyright © 2018 Kollmorgen |
|