AXIS#.HOME.MODE
Description
AXIS#.HOME.MODE specifies the homing procedure of the drive. The homing modes available in the drive are summarized in the following table. See Homing
The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position for a detailed description of each mode:
| Mode | Description |
|---|---|
|
0 |
Current position |
|
1 |
Find limit switch |
|
2 |
Find limit switch then find zero angle |
|
3 |
Find limit switch then find index |
|
4 |
Find home switch |
|
5 |
Find home switch then find zero angle |
|
6 |
Find home switch then find index |
|
7 |
Find zero angle |
|
8 |
Find end stop |
|
9 |
Find end stop then find zero angle |
|
10 |
Find end stop then find index |
|
11 |
Find index signal, without any precondition |
|
12 |
Find home switch, including end stop detection |
| 13 | Absolute feedback |
| 14 | reserved |
| 15 | Find next feedback zero position |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS, using either a PAC
"Programmable Automation Controller"
PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 15 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HOME.MODE | 0x5008 | 0x2 | UINT | - | - | RW | False |
| AXIS2.HOME.MODE | 0x5108 | 0x2 | UINT | - | - | RW | False |
Related Topics
Homing
|
Copyright © 2018 Kollmorgen |
|