AXIS#.HOME.MOVE

Description

AXIS#.HOME.MOVE starts a homing move. AXIS#.OPMODE must be set to 2 (position mode) and AXIS#.CMDSOURCE must be set to 0 (Service).

AXIS#.STOP can be used to stop homing after it has started.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS, using either a PACClosed"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

AXIS#.HOME.MODE

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Homing

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen