DIO#.SOURCE

Description

Gets or sets the bi-directional output source for channel x when configured as a digital output (see DIO#.DIR).

Value Description
0 - User User controls the output value using DIO#.STATEU
1 - Action Table Action table controls the output value

Examples

Usage

When DIO#.SOURCE = 0 (User) and DIO#.DIR = 1 (output), then DIO#.STATE will be controlled by DIO#.STATEU.

When DIO#.SOURCE = 1 (Action table) and DIO#.DIR = 1 (output), then DIO#.STATE will be controlled by the assigned action, if any.

If DIO#.DIR = 0 (input) then the DIO#.SOURCE parameter is ignored.

Code

Changing output state with STATEU and then changing SOURCE to be action table with no action configured:

--> DIO1.DIR
1 (output)
--> DIO1.SOURCE
0 (user)
--> DIO1.STATE
0
--> DIO1.STATEU 1
--> DIO1.STATE
1
--> DIO1.SOURCE 1 //Action table
--> DIO1.STATE
0

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen DIO1.SOURCE 0x368A 0x5 USINT - - RW False
DIO2.SOURCE 0x368B 0x5 USINT - - RW False
DIO3.SOURCE 0x368C 0x5 USINT - - RW False
DIO4.SOURCE 0x368D 0x5 USINT - - RW False
DIO5.SOURCE 0x368E 0x5 USINT - - RW False
DIO6.SOURCE 0x368F 0x5 USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen