DRV.HELPALL

Description

This parameter retrieves all information about all parameters and commands in the firmware. In most cases, DRV.HELPALL returns the minimum, maximum, default, and actual value for each parameter and command. Exceptions include parameters and commands that do not have these values (such as AXIS#.EN ) or pure INFO commands (such as DRV.INFO).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Terminal

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen