AIN.OVWTHRESH

Description

This parameter defines the over voltage threshold for analog input. If AIN.VALUE is larger than AIN.OVWTHRESH, and AIN.MODE = 3 (user defined fault mode), an over voltage warning is generated.

General Information

Type

NV Parameter

Units

V

Range

-10 to 10

Default Value

10V

Data Type

Float

Start Version

M_01-13-09-000

Related Topics

Analog Input (pg 1) | AIN.MODE | AIN.UVWTHRESH | AIN.OVFTHRESH | AIN.UVFTHRESH

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen