AIN.UVFTHRESH
Description
This parameter defines the under voltage threshold for analog input. If AIN.VALUE is less than AIN.UVFTHRESH, and AIN.MODE = 3 (user defined fault mode), an under voltage fault is generated.
General Information
|
Type |
NV Parameter |
|
Units |
V |
|
Range |
-10 to 10 |
|
Default Value |
-10V |
|
Data Type |
Float |
|
Start Version |
M_01-13-09-000 |
Related Topics
Analog Input (pg 1) | AIN.MODE | AIN.UVWTHRESH | AIN.OVFTHRESH | AIN.OVWTHRESH
|
Copyright © 2018 Kollmorgen |
|