CMPx.MODEN
Description
This keyword enables or disables modulo functionality on CMPx.
An error will be generated if CMPx.SOURCE, CMPx.MODBOUND1, CMPx.MODBOUND2, and CMPx.WIDTH are not set prior to enabling CMPx.MODEN. If CMPx.SETPOINT is not set prior to enabling CMPx.MODEN, the compare will trigger at the last set value, or the default value of 0 if the drive has been power cycled .
CMPx.MODEN must be set before CMPx.SETPOINT.
Example
The following example enables modulo for CMP1.
-->CMP1.MODEN 1
General Information
|
Type |
NV Parameter |
|
Units |
None |
|
Range |
0 to 1 |
|
Default Value |
0 (Disable) |
|
Data Type |
Integer |
|
Start Version |
M_01-13-00-000 |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC |
Revision DA or higher |
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
| 53A6h/0 |
CMP0.MODEN |
M_01-13-00-000 | |
| 53ADh/0 |
CMP1.MODEN |
||
Related Topics
|
Copyright © 2018 Kollmorgen |
|