CMPx.SETPOINT

Description

Use this keyword to set the position value for a Compare setpointClosedSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach. This position value will be compared against a Compare source (CMPx.SOURCE). If they match, an output pulse is generated. A setpoint also requires a width (CMPx.WIDTH) and width type (CMPx.WIDTHTYPE).

A setpoint must be armed (CMPx.ARM) before it is active. If a setpoints value, width, or width type are changed after it has been armed, that setpoint will be automatically disarmed.

Example

The following example sets the value of setpoint 1 to one billion for CMP1.

-->CMP1.SETPOINT 1 1000000000

General Information

Type

NV Parameter

Units

Units depend on value of CMPx.SOURCE. See table below.

Range

Argument 1: 0 to 7

Argument 2: -9,223,372,036,854,775,808 to 9,223,372,036,854,775,808

Default Value

9,223,372,036,854,775,808

Data Type

Argument 1: Integer

Argument 2: Integer

Start Version

M_01-13-00-000

Units

CMPx.SOURCE Units
0 (FB1) Depends on FB1.PUNIT or custom units.
1 (FB2) Depends on FB2.PUNIT  or custom units.
2 (FB3) Depends on FB2.PUNIT  or custom units.
3 (PL.FB) Depends on UNIT.PLINEAR or UNIT.PROTARY
Rotary: counts, rad, deg, (custom units), 16-bit counts
Linear: counts, mm, µm, (custom units), 16-bit counts

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-ICClosed"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher
FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

34AAh/1 CMP0.SETPOINT 0 M_01-13-00-000
34AAh/2 CMP0.SETPOINT 1
34AAh/3 CMP0.SETPOINT 2
34AAh/4 CMP0.SETPOINT 3
34AAh/5 CMP0.SETPOINT 4
34AAh/6 CMP0.SETPOINT 5
34AAh/7 CMP0.SETPOINT 6
34AAh/8 CMP0.SETPOINT 7

34BAh/1

CMP1.SETPOINT 0

34BAh/2

CMP1.SETPOINT 1

34BAh/3

CMP1.SETPOINT 2

34BAh/4

CMP1.SETPOINT 3

34BAh/5

CMP1.SETPOINT 4

34BAh/6

CMP1.SETPOINT 5

34BAh/7

CMP1.SETPOINT 6

34BAh/8

CMP1.SETPOINT 7

Related Topics

Compare Engines

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen