CMPx.SOURCE

Description

Setpoints (CMPx.SETPOINT) are compared against Compare source values. The setpointClosedSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach must be armed (CMPx.ARM) for it to be compared against a source. If they match, an output pulse is generated.

Value Compare Source
0 Feedback 1 (FB1)
1 Feedback 2 (FB2)
2 Feedback 3 (FB3)
3 Position Loop Feedback (PL.FB )

The source must be set before CMPx.SETPOINT.

Example

The following example sets the source to PL.FB for CMP0.

-->CMP0.SOURCE 3

General Information

Type

NV Parameter

Units

None

Range

0 to 3

Default Value

3

Data Type

Integer

Start Version

M_01-13-00-000

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-ICClosed"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher
FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

538Fh/0

CMP0.SOURCE

M_01-13-00-000
5390h/0

CMP1.SOURCE

Related Topics

Compare Engines

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen